TPS7B4255-Q1: what is Application circuit used for Transient testing as per ISO std

Part Number: TPS7B4255-Q1

Tool/software:

As per datasheet P-1, device is automotive load dump protected

1. What application board circuit exactly used while the device was tested for Load dump transient?

Please share test board circuitry details with exact comp. values used white transient & other EMC test were performed.

2. In addition to load dump transient , which other Automotive std. ISO 7637 & 16750-2 test pulse are performed on the device ? please share reports & test pulse

3. Does this device OUTPUT pin can also sustain ISO 7637 transient pulse 1a,2a,2b,3a,3b,4,5a  if applied on Pin no.4 ?

If yes, what would be application circuit to pass the test pulse if applied directly on Output pin