Tool/software:
Hi team,
During customer application of UCC21550-Q1, there could be some short time UV of VCCI from 5V to 2V. At is condition VCC UVLO will be triggered, and VCCI pin input current will increase to up to 0.24A. Could you help us understand why when VCC UV, its current will increase? Is this dependent on the PWM input status or anything else? Will this cause device damage risk (such as exceeding input side power limitation)?
Thanks
Scarlett