BQ25792: BQ25792 switchen between load batt 0A and 63A

Part Number: BQ25792

Tool/software:

Hello,

We are ussing the BQ25792 in our product and it works fine. we read out over I2C the values and 1 of the 10 on this moment is then switchen every 2 a 3 seconds between no charges or full charges.

is there a reason for this behavior we change the part and the nit is gone. Must we do special set-up for the BQ25792 to start work with it.

We use 2 batt and a charge power of 1A with a TS NTC

best regards Erik