Tool/software:
Hi,
In section 9.1.7, the BQ78350-R1 performs EDV-based RC adjustments when Current() ≥ 3C/32.(the capacity of my battery is 12120 mAh and the other one is 9090 mAh).
However, I configured the Overload Current to 200 mA.
When the current is 120 mA, the update occurs as expected — there is an update of FCC.
Is this normal behavior? I would like to understand what is happening in this scenario.
Thank you for your assistance.