Other Parts Discussed in Thread: LM317A, LM317-N
Tool/software:
Hello,
Could you please help me for understand the use of the fromula VOUT+ = VREF (1 + R3/R1) + (IADJ × R3). Indeed this formula is not related with VIN?
In other terms : I want to use this channel with VBAT+ under 12V to have in the outuput 10V +/-5%. The output voltage regulation stayed within 0.1%
I have tested the initila conf of the EVAL board "LM317A-337N-EVM" with 8V input and the meadured output is 5V (R1 = 240 Ohms and R3 = 715 Ohms)
I want to keep R1 under 240 Ohms. So what is the formula to apply with VIN (+12V) to have in the output 10V? for define the R3 output
The R3 changed with 7K15 and when I apply 12V Input, I obtain 11,06V Output.
Note: the needed output current is low (under 100mA)
Thank you for your help