Tool/software:
Dear Sir
I have to use TPSM82912/3 in my design and also i need module for nrgative voltage like this part for +2.5V 500mA load
Can you suggest the any part no that can be used for negative voltage -2.5V 500mA output.
The input voltage range is from 8VDC to 20 VDC nominal voltage is 18VDC