Tool/software:
Dear Sir or Madam,
I have the same issue as another person in this forum - my implementation of TPS61094 sometimes does not charge the supercap. Significantly, it often stops at ~0.7V and would not go higher.
My setup:
Vin = 3.3V from solar panel
Vout = 3.3V
Vchg = 2.6V
Ichg = 350mA
EN = MODE = HIGH through diodes from Vin and Vout.
I have absolutely verified that V_solar = 6.5V, Vin = 3.34V, Vout = 3.34V, EN = Mode = 3.28V, Vsupercap = 0.799V, and there is no charging for many minutes, without any sign that it would resume. Even if I unplug Solar panel, essentially making Vin = 0, and re-plugging. Also, I have put 3mF electrolytic capacitors in parallel with solar, and with Vin, and it worked better, but at a load transient of 100mA on output, the TPS61094 hang again, and stopped charging, and could not be re-forced into buck mode even with Vin = 0. It was again when Vsupercap = ~0.7V.
Can you please check out what is going on, and if such unstable operation is to be expected?
Best regards,
Andris Igaunis