This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63002 in parallel?

Other Parts Discussed in Thread: TPS63002, TPS63020, TPS63000

Hi all,

We need Li-Ion to 5V to power up our application and we have determined to use two TPS63002 in parallel to get 5V/2A peak. We have set up a board, in which outputs of the TPS63002s are simply short-circuited. However, one of the TPS63002 starts to warm up (and more input current is drawn) even if there is no load. By the way, they are performing pretty well when used independently (that is not in parallel). Is there a specific consideration when using two TPS63002 in parallel?  Thanks in advance.