Other Parts Discussed in Thread: BQSTUDIO, , EV2400, EV2500
Tool/software:
I am using a bq41z50evm board with an EV2400 and using bqStudio.
The bqStudio version is 1.3.128
The 41z50evm firmware is TI's release from April, 2025.
In bqStudio, I look at Data Memory -> Settings -> DA Configuration
I select Import Defaults, and the DA configuration field is set to 0x0012, which is the correct default value.
I select "Write All" to write the default values I just imported. Then I select "Read All" and DA configuration field changes to 0xffff.
That happens to several other fields also: Temperature Mode, Ext Temperature Mode change to 0xffff, LED configuration to 0xb22, Temperature Enable to 0xbb8, etc.
Am I doing something wrong, or do I perhaps have a bad flash sector on the board, or is my problem to be found elsewhere?