Other Parts Discussed in Thread: LM74502, LM74800-Q1, TPS4800-Q1
Tool/software:
Hello,
I'm looking at the LM74502 for a reverse input protection with load turn-off. Looking at the package and suggested footprint, it seems like the pad to pad distance between the OV, source and gate is only 0.2mm. As the OV pin is closer to GND, for higher system voltages (e.g. 48V+), this distance is too low for my application which requires at least 0.5mm. Is there as solution for this? I've had a look at the LM74500 but it doesn't seem to support back-to-back FETs.
Best,
Vincent