This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC14141-Q1: We need an isolated DCDC converter with >2KV isolation

Part Number: UCC14141-Q1


Tool/software:

We need an isolated DCDC converter with integrated transformer, with12V input and 12V output. 1W output power is preferred, but 0.5W is ok. 

Our requirement is insulation of 2000V with a lifetime >100 years.

The parts I have seen are advertised as 5kV isolation but for >100years lifetime they have 1kV tolerance. If needed we can work with a different input supply. 

Thank you

Haydar