TPS546A24A: Constant Current operation during OCP?

Part Number: TPS546A24A


Tool/software:

Hello team,

My customer is looking for buck converter, which will output constant current (adjustable) during over current protection.
They don't want the device to go shutdown during OCP.

I found TPS546A24A can set the OC behavior to ignore or disable.

Questions

  1. Can this device behave CC mode during OCP?
  2. Is the current level set by "IOUT_OC_FAULT_LIMIT", average current? or peak current?

If TPS546A24A is not capable of this behavior, is there any device which can do that? (max required IOUT is 8A)

Best Regards,
Kei Kuwahara