This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61099: Max output current and the package information

Part Number: TPS61099


Tool/software:

Dear,

Please let me ask 3 questions about the TPS61099.

1.) In the first page of the datasheet, there are 2 types of packages, WCSP and WSON. However, on page 23 and onward, there are different package, DSBGA and WSON. Is WCSP as same as DSBGA?

2.) What is the difference between TPS61099 and TPS61099x?

3.) What is the maximum output current when Vin=3.3V, Vout=5.5V?

Regards,

Miatsu