TPS55288: Setting OE bit to 1 on TPS55288 is causing registers to reset

Part Number: TPS55288

Tool/software:

Hi, 
I have a circuit with the TPS55288, Vin is supplied by a ~3.7V LIPO battery.

EN/UVLO is above 1.23V via a transistor.
I can communicate with the IC over I2C just fine at 75h.

But when setting the OE bit to 1, all of the registers get reset at the Vout is ~1.85V.
VCC is measuring ~3.4-3.5V.
There is no fault reported on register 07h. It reads as 0x01.

My schematic is attached below.