This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5146: Can it be used for GaNFET

Part Number: LM5146
Other Parts Discussed in Thread: LM5116, LM5113

Tool/software:

Hi team,

My customer is using BUCK controllor LM5146/LM5116 for GaNFET in BUCK application.

Input voltage is 48V normal/100V max. Output is 12V/18V/24V 20A.

Can LM5146/LM5116 be used for GaNFET? Or customer should only use LM5113 such pura half bridge driver.

If LM5146/LM5116 can do it. Are there any design notice. And are there any successful story or TI reference design to use LM5116/LM5146 to driver GaNFET.