Other Parts Discussed in Thread: TPS37
Tool/software:
I Want TPS3700 IC DSKR Package
Suggest me Part Number for the same
OV = 16V
UV = 8.5V
Hysteresis = 3%
Available on Digi key or TI Link for Exact Part Number
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
TPS3700 only has DSE package (6-pin WSON) package, and is available with adjustable threshold (OV = 400mV, UV = 394.5mV) only. The exact part number is TPS3700DSER.
TPS37 does have a DSK package (10-pin WSON), but we do not have a variant with fixed 16V OV threshold and 8.5V UV threshold currently available. We do have an adjustable variant, TPS37A010122DSKR, which can be set to any thresholds using external resistors. This device has 2% hysteresis.
-Henry