This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54308: Schematic revive request

Part Number: TPS54308


Tool/software:

Hi team ! I'm trying to design 8.5V~5.5V battery to 5.2v 2A converter with the mentioned buck regulator. Reason I asking is that webench simulation and data sheets recommended schematics has used  different values of inductor and feedback resistor configuration. According to the webench used 6.2uH inductor and 13.3K ohm but in datasheet FB resistor value calculation. But that come with 6v output according to the datasheet calculation.
 

  • Hi Amarsai,

    Schematics seems fine but there are few changes need to be made,

    Rbottom needs to be 13K ohm to get an output voltage of 5.2V.

    As, Vout = Vref(1+Rtop/Rbottom)

                  = 0.596(1+100/13) ~ 5.2V

    With 18k ohm you will get an output voltage around 3.9V.

    Best regards,

    Usha.