Other Parts Discussed in Thread: LSF-EVM
Tool/software:
After having watched to the LSF family video "Down Translation with the LSF Family"
At 2'30 it is said :
"If the leakage current into the receiver is less than 1 microamp, then the resistor RA1 can also be removed."
I don't understand why we couldn't remove the pull-up resistor when there are some significant leakage, or even big leakage.
My basic reasoning is that the mosfet is bidirectional, so the Drain and Source can be swapped. If ever, because of leakage at A side, (and no pull-up RA1) the voltage would decrease, the MOSFET will conduct, the Source being on A side and Drain on B side. So the voltage cannot not colapse on A side, even with significant leakage, and RA1 is not needed even if there are significant leakage.
I do a test on LSF-EVM with VrefB=5V, VrefA=3.30V, on side B a 1 level (5V) and no pull-up on side A
If I measure the output A with my multimeter Fluke 87V (10Mohm impedance), I measured 3.49V... so a bit higher than the expected 3.3V.
If I put a 10kohms pull DOWN on A side, creating a 330uA !! leakage, I measure 3.19V, which is still a good 1 level.
If I put a 10kohms pull UP on A side (and no pull-down, no leakage), I measure 3.37V, a bit higher than 3.3V
So there is a leakage from B side to A side which is attenuated by the pull-up or the pull-down. (same kind of leakage than we can see on VrefA pin)
At the end, I would think that the advice to keep the A pull-up when there are some leakage and to remove it when they are no leakage is just the inverse of what should be done, isn't it ? :-)
I would likely change the advice to "If the leakage current into the receiver is less than 1 microamp, then keep the RA1 resistor or add a pull-down to increase leakage." In that way, the voltage on A side will not go too much about VrefA. A 100kohms pull-down is perfect is the above case.
Am I right ?