This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR54406: COUT calculation (equation 11 and 12) is strange

Part Number: LMR54406


Tool/software:

Hello team,

From the datasheet equation 11 nad 12, I get different result compared to what is stated on the datasheet.
Could you double check?

The datasheet says COUT no less than 2.38uF, but if I calculated using datasheet chosen value, the result is 1.52uF.
I used datasheet parameter: (VOUT_C = 30mV, KIND=0.4, IOUT=1A, fsw=1100kHz)

Also the result of equation 12 seems to be different from my calclation.

The datasheet says COUT no less than 14.3uF, but if I calculated using datasheet chosen value, the result is 9.09uF.
I used datasheet parameter: (IOH=1A, IOL=0A, fsw=1100kHz, VOUT_SHOOT=400mV)

Best Regards,
Kei Kuwahara