Tool/software:
Hello,
We have the following design specifications.
Input voltage range: 9-80V
UVLO 18V
OVLO 36V
OC trip: 100A
Reverse Voltage Protection - 50V
Short Circuit Protection
Fault or PG output
It looks like the TPS4810-Q1 part will be able to meet all of these requirements (with parallel FETs) except the OVLO.
Is it possible simply to add a OVLO to this IC?
Maybe using the control inputs (INP1/2)
Thanks in advance,
Nick