Tool/software:
I am trying to simulate a full H-bridge driver driving a capacitive load. It is expected to develop a 40V peak-peak square wave across the load capacitor. However, it does not work (gives 0 output) even though the half-bridge version of the circuit seems to be working. The voltage at HO outputs is a DC of about 17V. The schematic and simulation is attached. The VDD voltage is 9V and the input voltages applied at HI and LI input are 3.3V complementary clock. The high-voltage supply is 20V. The clock frequency applied the input is 2.5 MHz. Requesting help.