Tool/software:
Hi there,
We are using the BQ25798 and need higher voltage at Vsys for system and battery both.
According to our configuration, which uses a single-cell battery, we have set the registers through the PROG pin, and we correctly get 3.7 V at VSYS, as expected.
Since our entire system depends on VSYS, we need a higher voltage when VBUS is connected. To achieve this, I programmed the REG00_Minimal_System_Voltage register with values corresponding to 9 V (0x1A) and 12 V (0x63). The VSYS voltage does rise to the desired value, but only for a few seconds before dropping back to 3.7 V.
Interestingly, when I read back REG00, it still shows the value I set for 9 V. I have also disabled the watchdog timer, but the issue persists.
Could you please help us understand what might be causing this behavior? Is there something we might have missed?
This issue is critical for our design.
Best Regards,
Pratham