Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQ34Z100EVM, , BQSTUDIO, EV2400, BQ34Z100
Tool/software:
I’m using a bq34z100EVM board attached to a battery pack that I want to monitor with the bq34z100-G1.
I have configured part of the parameters related to my project, but I still need to make some modifications because I am in the evaluation stage.
The ChemID selection was done using the Chemical ID Selection Tool.
I then started the learning cycle as described in SLUA903.
However, once the IT_ENABLE command is sent and QEN is set, I am no longer able to modify anything in the Data Memory.
I can unseal the device (SS bit cleared, FAS set), but I cannot gain full access (FAS = 1).
Even in this state (unsealed but not full access), I cannot modify any information in memory.
Is this a normal situation?
I still need to modify and configure the behavior of some circuits on the EVM board (such as LED, ALERT, and others), but everything seems locked.
Is this expected behavior, or did I do something wrong?
I also tried to program the image I saved before entering the learning cycle, but it is not possible without full access.
Any ideas?