This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2373: recommended isolated PoE PD IC, 5V output @ 1.8~2.2A + ref. schematic & BOM

Part Number: TPS2373
Other Parts Discussed in Thread: TPS23758

 

Dear Sir/Madam,

I am currently designing a product based on the ESP32 with Ethernet connectivity. The system will drive an 8-channel 5 V, 30 A relay module (each relay rated at 5 V, 30 A).

To support this design, I am looking for a suitable isolated PoE IC that can provide a 5 V output at approximately 1.8~2.2A. Could you please recommend an appropriate IC (or family), along with any available reference schematic, BOM, or evaluation board that I could adapt for my design?

Thank you very much for your time and assistance.

Best regards,
P. Mahesh