This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25798: Spec and test comparison

Part Number: BQ25798
Other Parts Discussed in Thread: BQ25790,

Hi expert,

We are promoting BQ25798 to replace BQ25790 in INSTA360 and keep TI's share. Customer want TI to provide the spec and test comparison between BQ25790 and BQ25798. I can't find any comparison in Seismic. Could you help to provide some detailed comparison? Thanks.

Best Regards,

Ryker

  • Hi Ryker,

    BQ25790 is the parent of BQ25798.  BQ25798 inherited all of the registers and has some new ones as highlighted below.  Efficiency is the same as you can see from the datasheet efficiency curves.

    SPEC/FEATURE 790 798
    package WCSP QFN
    Converter shutdown for 30ms after OVP due to missing battery Yes No
    MPPT No Yes
    Backup mode  No Yes
    Option to disable charge after WD timeout No Yes
    IBAT pin with voltage proportional to current Yes No
    BATN pin for remote PACK- sense Yes  No

    Regards,

    Jeff