Other Parts Discussed in Thread: LM25139, LM25149, LMR51403
Hi. I have been looking for a microcircuit for several days and can not decide on the choice.
Main parameters: Input voltage 33 V
Output voltage 13 V
Output current 10-200 mA
Current limit mode is required. So that the output current does not exceed 200 milliamperes.
I also plan to use UVLO and PFM
the most successful option is LM25139
But there is perhaps another solution. Perhaps there is something with integrated transistors?