Dear TI Support,
I am currently designing a circuit using the TPS54531DDAR.
In the datasheet's "9.2 Typical Application" section, multiple bypass capacitors (e.g., C1, C2, C3) are connected in parallel at the VIN input.
To reduce BOM cost, I would like to reduce the number of bypass capacitors, while keeping the total capacitance unchanged (for example, changing from 3 × 4.7 µF to 1 × 10 µF).
Could you please advise on the impact of reducing the number of capacitors in this way, specifically regarding device performance, stability, or noise characteristics?
Also, if such a change is acceptable, are there any points we should pay attention to in terms of component selection, ESR, layout, etc.?
Thank you very much for your support.
Best regards,
Ren