This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3.5kW PFC without input Rectifier Bridge, using UCC28070

Other Parts Discussed in Thread: UCC28070

Subject:  PFC--3.5kW using UCC28070 Interleaved input Bridge & Bridgeless

kindly send me the excel design tool for PFC using UCC28070.

i already have " UCC28070 Design tool 8 15 08 " ---but this is with a single controller.

i want the design tool using 2 nos. of controllers with 180 deg. phase shifted. + i want the design tool using 2 nos. of controllers with 180 deg. phase shifted for a BRIDGELESS PFC  design.

Rajesham.E.

Triport Energy Systems

93472 56728 / 9140 2794 0197