Other Parts Discussed in Thread: , BQ25690
Hi, we are developing a product where we need to charge a 3S battery from a 12V source at 2A and, when the device is out of its charging station we need it to boost the battery voltage to 24V 1.5A to power an external load. For this we selected BQ25756 because of it's features and the ability to change charging parameters using i2C.
As this is our first design using a bidirectional full bridge topology we have some questions regarding the design procedures given our dissimilar working conditions.
On the datasheet a desing procedure is described for a charging application. However we couldn't find any example or application notes explaining a design validation for the reverse output or step-up functionallity.
We understand IC's limitations regarding mosfets selection, inductor max values and working modes. Most of it's securty features will be replaced by a battery fuel gauge so we only need it to charge and boost output.
Are there any resources that we could access to aid on our design? Sorry if this question has been asked before, we checked and did not find any.