This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25690: Looking for Standalone 2S Li-ion Charger IC with High VIN (and regulated output when battery absent)

Part Number: BQ25690


Hello E2E Experts,

Good day.

I am designing a charging circuit for a 2-series Li-ion battery pack, and I would like to find a suitable TI charger IC that meets the following requirements:

The charger board must be able to power the system load and charge the battery in all three combinations:

Battery present / VIN present
Battery present / VIN absent
Battery absent / VIN absent

Specifically, when the battery is absent but VIN is present, I do not want VIN to be directly passed to the output (i.e. VIN should not connect directly to VOUT).
Instead, the output should be regulated to a voltage close to the nominal battery voltage.

The input supply (VIN) may be around 36 V or higher, so the IC must tolerate a high input voltage.

Could you please recommend an alternative TI charger IC that supports:

2S Li-ion battery charging,
Standalone operation (no MCU required),
Regulated output when battery is absent, and
High VIN tolerance (~36 V or more).

During my research, I found the BQ25690, which seems to meet many of my requirements, but I could not find sufficient documentation, application notes, or design resources about this part.

I would like to know whether the BQ25690 is suitable for this type of system, and if so, could you please share additional application notes, detailed datasheet, or reference designs related to this configuration?

Regards,

TICSC

  • Hello,

    The BQ25690 is a very new part, so there is not much documentation on the device yet.

    Battery absent / VIN absent

    Where would the board be getting power from in this instance? Our chargers cannot power the board without a power source.

    The input supply (VIN) may be around 36 V or higher, so the IC must tolerate a high input voltage.

    The BQ25690 input operating range maximum is 36 V. The device can tolerate higher input voltages, but it will not switch at voltages higher than 36 V.

    Best regards,
    Michael Bradbourne