TPSM843321: Line Regulation Specifications

Part Number: TPSM843321


Dear Sirs and Madams,

 

We are considering using the TPSM843321.

Input voltage: +5V to +12V

Output voltage: +4.5V

We are considering dynamically switching between +5V and +12V input voltage. 

This module has a maximum duty cycle of 98%, so I understand that it is no problem to generate an output voltage of +4.5V from an input voltage of +5V, but the datasheet does not specify line regulation. 

Could you please provide us with information regarding line regulation? 

Regards,

Masashi