Part Number: BQ25672
Other Parts Discussed in Thread: BQSTUDIO
Hi team,
My customer is now considering the configuration of BQ25672.
And they have following question. Could you please support it?
________
We understand that in the our application, various parameter thresholds can be configured by writing to the registers via software and then transmitted through the communication port to update each parameter.
Are the adjustable parameters those listed in Section 8.5.1 “I²C Registers” (addresses 0h to 48h, total 57 items) in the datasheet?
Also, regarding these registers:
• Do you have any sample code or reference for how to set and transmit the register parameters?
• Once the parameters are written to the registers, are they applied only before charging starts, or can they be updated dynamically during charging operation as well?
________
Best regards,
Goto