I'm using bq27510-G2 on another project with a lithium ion battery. Is it possible to use one of these gauges with a CR123? Its a primary Li/MNO2 battery. I'm not completely sure how the learning process / chemistry selection works. I suppose if I went through a cycle with the CR123 and it was close enough to a Li-ion that might work. I doubt that will be the case however because CR123s have OCV around 3V and cutoff around 2V.
Any ideas?