This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61480: Suitable device recommendation

Part Number: LM61480
Other Parts Discussed in Thread: LM65480-Q1, , TPS62918, LM61495

Hi expert,

My customer has a BUCK device request, please help to recommend suitable devices. Thanks.

  • Input voltage 3 ~ 12 V
  • output 2.8 V
  • 5‑8 A witn minimum input voltage 3.2 V
  • Must support FPWM mode
  • Output OVP (Nice to have): The output side may be connected to a voltage source higher than the set value, and the chip can not be damaged or back‑fed. 

Best Regards,

Ryker