Hello,
The LT-SPICE 24 simulations of the LM43601 configured to output neg12V from a pos15V input failed so far.
I am using the following LM43601_AVG.LIB model which I believe is correct.
The schematic is identical to the one proposed on Webench.
Any idea on what could explain the simulation failures?
Thanks!
WEBENCH design proposal:
LT-SPICE 24 design proposal: