My system has a primary power source that is a vehicle
battery voltage (12-14V typ), but I need a second power source to
supply the circuit when the primary source is not active.
I have planned to use a Li-ion (1 cell) or NiMH (3 cells) batteries as second source.
When the vehicle battery is present, It must supply the current for theLi-ion battery charge + system load current (<=200mA).
When the vehicle battery is not present, the Li-ion battery must supply the system load
I have a doubt about which topology I must use.
The first one is to put the system load in parallel with the Li-ion Battery and use a simple charger IC. At the same time that I charge the Li-ion battery , I am supplying the load. My doubt is about how the charging process of the battery (constant current - constant voltage) is affected by load current in parallel.
The second topology is to use a Smart Power selector IC (like MAX8934 for instance). So the Li-ion charge process is controlled by this IC and the load current can be supplied from the main vehicle battery when it is present and from the Li-ion battery when it is not present.
Of course, the solution must be as cheap as possible and with the minimum PCB size.
Some recommendation? TI has some circuit or application note that can help me? TI has some Smart Power Selector Circuit or similar?
Thanks in advance