Hi,
While seraching for a method to measure the state of charge of my LiSoCL2 battery pack (3 in parallel Saft LSH20) I found the BQ35100, which seems suitable for the job. I just have a few question before proceeding with the HW for it:
1. In the datasheet is recommended to use the EOS mode for this battery kind. While In this mode can I still figure out the percentage left on the battery pack? My use case would be to report every 8 hours the battery state
2. The three battery in parallel gives me 39 Ah capacity, is this ok for the BQ35100 ?
3. Any other thing I need to have in consideration ?
Thank you!