This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

15V split rail supply design recommendation

Other Parts Discussed in Thread: REF102, TPS54060, TPS54060EVM-590

Hi!

In my recent design I'd like to use an inverted REF102  to get a -10V reference to an MDAC. There would be an I/V converter step after the MDAC, too. In the same design there would be a digital circuitry drawing maximum 50mA current at regulated 3.3V and I also need a low current 5V regulated source to supply an USB-Serial bridge chip. The main power source would be a 24V wall adapter.  In summary:

  • +/- 15V clean rails
  • +5V for USB-serial bridge
  • +3.3V for MCU, LCD display w/ backlight etc

For the inverting step I found this note which looks promising:  link. However,  I'd welcome any recommendations in the first steps as there are lots of possible ways to create such a power supply environment. Thank you!