This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22953: TPS22953 maximum current

Part Number: TPS22953

Hello,

I plan to use a TPS22953 as a power switch to supply a  device with a maximum current of 3A.

The TPS22953 is powered with a current-mode controlled DC/DC power supply. The current limit of the power supply  is 5.8A typ, 7.25A max.

How will the TPS22953 behave in the event of overcurrent (> 5 A) or a short circuit in the device? 

Best Regards