Part Number: BQ25882
Hi team,
For BQ25882, when VBUS is not supplied and current flows from BAT to SYS, could you please provide the maximum current that can be delivered in this state, both for continuous current and peak current?
I have seen in other E2E threads that the maximum discharge current is 5A, but the datasheet states a maximum of 4A. Are these values referring to continuous current?Please clarify the continuous current and peak current specifications.
Also, regarding the output capacitor, the datasheet recommends 44µF, but what is the maximum allowed value?
Best Regards,
Shota