This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62840: RDS(on)

Part Number: TPS62840

Hi Experts,

The TPS62840 datasheet shows high-side Rds(on) typical values versus temperature (Figure 6), as well as maximum values for Vin of 3.6 V and 5 V.

1. Could you please provide data on high-side Rds(on) maximum values for lower Vin (2 V, 2.2 V, 2.5 V and 3 V)?

Regards,

Marvin