Hi !!!
At page 12 of bq2060A datasheet, I read "FCC becomes invalid if it is initialized or updated to a value less than 256mAH."
What does it happen into the BQ2060A if, using a damaged 400mAh Lead Acid Battery, FCC is updated to a (real) value less than 256mAH ???
At the first Qualified Discharge, FCC has been updated to a correct 250mAh value ... but, after a full charge (to the real 250mAH battery capacity) and a second Qualified Discharge, FCC was updated to 65530mAH value (equals to a 16 bits unsigned integer 250-256 !!!). After a third full charge and qualified discharge, FCC was updated to 65274mAH (65530-256 ...) and the gas gauge has become unusable !!!
Is it possible to avoid this problem in any way ???
Here is the .LOG file
Thanks a lot,
Giovanni