This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: BQ34110 Load Learning

Part Number: BQ34110
Other Parts Discussed in Thread: BQ34Z100,

I have an application where I have a 19.2V, 96Wh LiFePO4 pack charged with a solar panel.  It will drive a load on a daily basis - which might might drain it by roughly 10%.  In general, it should rarely fully discharge.

I have 2 questions:

  1. In this case, is the BQ34110 the prefered solution over the BQ34Z100?
  2. If the BQ34110 is preferred, is it necessary to include a learning load, or can the LEN pin be left disconnected?

Thanks