What is the maximum allowable TPS62140 output capacitance?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TPS62140 is an internally compensated switching converter. In general, the user must properly select the external filter components (output inductor and capacitor) to be stable with the fixed internal compensation. Each specific IC's datasheet contains information on the allowable component selection. An appication note on the TPS62140 allowable external components provides even more indepth information. The title is "Optimizing the TPS62130/40/50/60/70 Output Filter" http://www.ti.com/lit/an/slva463/slva463.pdf
This application note is referenced in the datasheet and is also in the TPS62140 technical documents.