This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: Driving motor with increased current

Part Number: TPS1663
Other Parts Discussed in Thread: TPS1686

Is it possible to use an eFuse (i.e. TPS16630) set the current limit to 2A, however, start a motor which requires for a short timeframe ~4s an elevateed current of 5A?

Any recommendations for such a circuitry?