This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS758: EOL

Part Number: TPS758

Hi Team,

I have selected TPS75801KTTRG3 for my design to convert 5V-3.8V. i will be needing this Part for next 10 years. Will it be active.

  • Hello,

    This device is not actively on EOL status, however given that it is one of our older devices it is recommended to use one of the newer gen devices specially for a project with a long lifetime. One newer gen recommendation would be TPS7A5301RPSR which can also handle up to 3A load current.

    Quick spec comparison below for reference:

      TPS7A5301RPSR TPS75801KTTRG3
    Iout(Max)(A) 3 3
    Vin(Max)(V) 6.5 5.5
    Vin(Min)(V) 1.1 2.8
    Vout(Max)(V) 5.15 5
    Vout(Min)(V) 0.8 1.22
    Fixed output options(V) ADJ ADJ
    PSRR @ 100
    KHz(dB)
    28 12
    Noise(uVrms) 4.4 35
    Accuracy(%) 0.5 3
    Dropout voltage
    (Vdo)(Typ)(mV)
    60 150
    Iq(Typ)
    (mA)
    2.8 0.12
    Output capacitor type      Ceramic Non-Ceramic
    Thermal resistance
    θJA(°C/W)
    46.5 39
    Operating temperature
    range(C)
    -40 to 125 -40 to125
    Package size: mm2 5.5 mm2: 2.5 x 2.2 (VQFN-HR|12) 155 mm2: 15.24 x 10.16 (DDPAK/TO-263|5)
    Rating Catalog Catalog
    Features Enable, Foldback overcurrent protection, Output discharge, Power good, Soft start Enable

    Regards,

    Andres