This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC33063A: VREF Accuracy over temp

Part Number: MC33063A

Is there a similar diagram as below to show the precise VREF over temp?

 

NCP3063.png

 

 

 

  • Hello Brian,

    We do not have such a typical characteristics graph over temperature. Please do not forget that this is just a typical graph, only the values in the electrical characteristics give the real behavior over temperature and production. Not the typical graph.

    Best regards,
    Brigitte

  • In the datasheet, it mentions the 2% internal reference; is this specified over the temperature range or at 25 degrees? It isn't clarified in the E/C table.

    What customer concern is the variation with this reference voltage over temp!

    Regards

    Brian

  • Hello Brian,

    Please check the section 7.7 in the datasheet. You find in this section the value at room temperature and as well the full temperature values we guarantee.

    Best regards,
    Brigitte