This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Soft-start control of LMZ10501

Other Parts Discussed in Thread: LMZ10501, LMZ10503, LM2852

Hi all,

I was wondering if anyone has experience in using the soft-start features of the LMZ10501 module. I understand that this is a National part, but they don't have a forum, and LMZ1051 announcements have already been made on this forum...

The datasheet makes it seem that soft start is not configurable, the way it is with something like the LMZ10503. However, that whole line is much larger than the LMZ10501... Nonetheless, Webench classifies the LMZ10501 as a regulator with controllable soft start. Does anyone know how to set that? I want to have a 3.3V to 1.5V conversion start-up take between 2-4ms, as opposed to the 70us that it took on the Startup plot on pg. 8 of the LMZ10501 datasheet.

Thanks for any and all help!