This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92360: Efficiency Data vs. Iout

Part Number: TPS92360

Hi support team,

Is there a graph showing the load (Iout) and efficiency when using 6 LEDs?
Figures 8-2 to 8-5 in the datasheet show the efficiency for dimming duty with RSET = 10.2ohm  (Iout = 20 mA).
I would like to confirm the efficiency under the following conditions.

Vin: 3.3V
Vout: 18V (Vf=3V, 6 in series)
Iout: 3mA

Regards,
Dice-K