This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2121: TPS2121 "seamless" vs TPS2117

Part Number: TPS2121
Other Parts Discussed in Thread: TPS2117

Hi all,
I am design a board and would like to replace the tps2121 by the tps 2117 (lower quiescent current).

I ack that there are differences in many parameters : voltage, RDson, ...

I checked all of them but I still have one question about the "seamless" of the 2121 that isn't present in the 2117.

I implemented an automatic priority mode (see picture):

image.png

My understanding is that the only difference in behavior is that with 2121, if VBATT (IN2) were to drop below P5V0 (IN1), 
IN1 would be selected back, which won't be the case with 2117 as IN1 is compared to internal (1V) reference ?